Other Parts Discussed in Thread: DRV8701,
Hello,
I finally used the TS5A23166DCUR for the application but it don’t run as I thought….
I have the schematic of the figure.

With 2,5V in Vref, if the LDO turn off, VCC should be 0V, but I have around 1,29V… and this voltage varies with Vref (in COM1). If Vref is less than about 1,9V, then VCC is about 0,7V and below of this Vref value, Vcc goes to 0V and the TS5A23166DCUR switch off correctly.
It appears that the voltage of COM1 >2V drain to Vcc and supply the TS5A23166DCUR.
I was hoping that with ldo off, TS5A23166DCUR goes to high impedance. What could be happening?
Thank you!