Other Parts Discussed in Thread: TMUX7236
This post is made to warn designers wanting to use the TMUX6236 as there is an error in the datasheet.
The datasheet was downloaded though the TI website via this link: https://www.ti.com/lit/ds/symlink/tmux6236.pdf?ts=1707141302799 on 06-febr-2024
I have marked the errors I have found in the WQFN package, but I have seen errors also in the TSSOP package. see screenshot below.
I would appreciate if the datasheet can be corrected.
On the page of the TMUX6236 the TMUX7236 is stated to be a drop-in replacement of the TMUX6236
The TMUX7236 seems to have a matching chip pinout with the pinout stated in the datasheet, I assume this is also the pinout that should have been shown in the datasheet of the TMUX6236. But confirmation of which one is correct would be appreciated.