Other Parts Discussed in Thread: TMUX1574, TPS2116, TMUX1108, TMUX1308
I'm using a TMUX1208 powered by 5v to multiplex a 3.3v VCC wire from my modem to the source but it’s possible that voltage/current becomes unstable after 3 hours.
The modem I’m using will shut off if it detects the 3.3v connection is unstable. I was using the TMUX1574 just fine, no disconnects or interference. I've been able to pin point that it's the TMUX1208 by hardwiring the VCC wire to the source (bypassing the TMUX1208) with no issues.
So basically if the tmux1208 fails to supply enough 3.3v power to the source then the modem will shut off and require a reboot.