Part Number: TMUX4827
Other Parts Discussed in Thread: TMUX6236, TMUX2889
Hi,
Our customer is looking for a MUX that can switch 125KHz/134kHz, 10Vpp signals, can we use the TMUX4827?
According to "Figure 6-22. Maximum Signal Swing" in the data sheet, it appears that the amplitude is limited to 2Vmax for inputs over 50kHz.
As a result of actual customer trials,
When inputting a signal of 10Vpp_100kHz, the output from D1 is attenuated to 6Vpp.
Please let me know if there is a MUX that can be used with single power supply 5V, 125KHz/134kHz, 10Vpp input/output.
Or does TI recommend a MUX with Vss > 10V ?
Best regards,
Hiroshi