This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX131: Can TMUX131 be used to as USB2.0 multiplexer?

Part Number: TMUX131
Other Parts Discussed in Thread: TS3USB3000,

Hi,Team

TMU131's bandwidth is 6.5G.Can TMUX131 be used to as USB2.0 multiplexer( The function is similar with TS3USB3000 except of channels)?

  • Hello Ken,

    The TMUX131 can support any input signal from 0 to 3.6V(just like the  TS3USB3000)   and should work fine with an input signal frequency of 480Mbps (240MHZ) which is the USB2.0  standard.

    Please let me know if you need any additional assistance!

    Regards,

    Kameron