This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV4066A: About Vcc

Part Number: SN74LV4066A
Other Parts Discussed in Thread: TMUX1111

Hello Team

I have a question regarding Vcc for SN74LV4066A.

The Features and Description sections on page 1 of the SN74LV4066A datasheet state "1.65V to 5.5V VCC operation."

However, on page 5, under the "5.4 Recommended Operating Conditions" section, it states "VCC Supply voltageMin 1V Max 5.5 V."

Which one is correct?

Best regards,

Tomoyuki