Hi all,
We are having a issue in our product where input source control (0-10 volts) to analog switch is low powered (5 mA) and output of analog switch is connected to other device which is high powered device (10mA).
I want to know how much each channel can sink when it is connected a low powered input and high powered output which is trying to sink more power (10 mA).
We want to know which type of buffer or switch will work in this situation.
Please help.
Thanks in advance.