Other Parts Discussed in Thread: TPS22810
Hi,
Does TMUX8211 can be use to switch power rail such as to select +48V (s1 to d1) or -48V (s2 to d2) ?. Thank you.
Regards,
Harris
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Harris,
Like Clemens said, in theory you could definitely do this. I would recommend seeing if the current limiting effect of the Ron of the switch negatively affect your application.
If a power/load switch is preferred then I can move this thread to that group. Maybe they have something in the roadmap for negative voltages.
Regards,
Alex
Hi Harris,
Can you share details of your requirement like voltage, current and protection requirements. What is EE and application?
Regards
Kunal Goel
the requirement:
Voltage: +/- 48V
Current: +/- 200mA
Application for High voltage amplifier
Hi Harris,
Presently we don't have integrated solution for -ve voltage. You can check -ve hotswap which needs external FET.
Regards
Kunal Goel