This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3126: SN74CBTLV3126RGYR spec question

Part Number: SN74CBTLV3126

Does this part support I3C?

Can you provide detailed specs about rising and falling?

Part: ANALOG SW. SN74CBTLV3126RGYR VQFN14

  • Hi Aceline,

    Thanks for reaching out here. Based on the device parameters, it seems that it could be used to support I3C given low Con, decent bandwidth and voltage support up to 3.6V. You can find more info on choosing an I3C part with our FAQ.

    Unfortunately, I don't have access to details specs for timing outside of what is already in the datasheet due to this being an older part. 

    Regards,

    Alex