1、SCH

2、 S0=1,S1=0,1OE=0,2OE=0

3、The output level is related to the output pull-down resistance, and the test waveform is different for different pull-down resistance

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、SCH

2、 S0=1,S1=0,1OE=0,2OE=0

3、The output level is related to the output pull-down resistance, and the test waveform is different for different pull-down resistance

Hello dang,
Please checkout this e2e post which explains more on this topic as I believe I answered a very similar question yesterday!
Regards,
Kameron
Kameron~Thanks a lot
"So the reason why you are seeing this behavior is because the pull down resistor of 10K is sinking a large amount of (3.3V/10K= 330ua) current and affecting the Ron of this device"
-----Can you explain in detail how the sinking current is affecting Ron?
------TI's level shifting chip has a similar phenomenon?Whether there will be leakage current if there is a pull-down resistor?
---- Is a p2p replacement for the SN74CB3T3253 device (FET only and no level shifting)?
Hello Dang,
1. So section 5.4 off this appnote explains in greater detail how the Ron CB3T devices works. A simple rule to remember for this device is "As the output current increases, Ron decreases.
These graphs from the datasheet show what I mean in greater detail.

2.All Ti analog multiplexers in the CB3T family will have the same phenomenon when there is a pulldown resistor( there will be "leakage" current) If you would like to know more about other TI translator devices I can forward this thread to another team.
3.Yes SN74CB3T3253 is a normal FET without the level shifting. For example if your supply is 3.3V when you pass a 3.3V signal in you should see approximately 3.3V on the output.
Please let me know if anything is confusing and I am happy to help in any other way needed!
Regards,
Kameron