This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3Q3306A-EP: Hi-Rel Analog Switch application.

Part Number: SN74CB3Q3306A-EP
Other Parts Discussed in Thread: TS5A23157, TMUX6201,

Am switching LED Cathode (for connect and disconnect of LED current to another circuit) using CCB3Q3306AMPWREP. The datasheet says it for analog as well.

Slightly worried. am confident that TS5A23157 or TMUX6201 can be used as it is a bidirectional analog switch.

Am planning to use CCB3Q3306AMPWREP/SN74CB3Q3306A-EP for the Aerospace recommend use, it there is a PSPICE file i would have simulated it.

Can anyone let me if i can use a LED Cathode to Pin A and Get same signal as pass through on Pin B when i control OE