Other Parts Discussed in Thread: TS5MP645,
We are using multiple TMUX646 devices in a cascaded format to create a 4:1 multiplex of a 100 ohm diff pair. Unfortunately we are seeing a lot of losses in our system, which ramp up significantly above 100MHz. I note that this is the latest greatest of the TI high speed multiplexers, but I also notice it has a significantly higher Rds on than its previous generation part, the TS5MP645 ( 6 Ohm vs 2.45 Ohm).
Our implementation is actually attempting to drive an RJ45 cable and measure cable performance parameters such as crosstalk, insertion loss, return loss. It requires 3 MUXes cascaded. We require very low crosstalk in the MUX, such that we can measure crosstalk of the cable without nearing the noisefloor of the MUXes. The drive signal is sent through the cable under test and then looped back onto an adjacent pair, so the signal propagates through 6 MUXes before being terminated. The muxes are such that we can drive each cable pair one at a time. They are wired in such a way that if they are not being driven, they are being terminated at 100Ohm (the 110 Ohm on the schematic is in parallel with 1K on the signal measurement device).
We chose the TMUX646 over the TS5MP645 due to its better crosstalk performance. However, we are having problems above 100MHz where the losses are larger and affecting our measurements. My question is, do you think we would get reduced loss up to 250MHz if we chose the TS5MP645 ? Due to the nature of the package it's not easy to swap the devices by hand, but our PCB assembly house is confident they can swap them for us if you think there may be a reduction in power loss with the TS5MP645 ?
I would have thought that the compound loss of the 6 Ohm RDSon x6 (3 drops on the way out and 3 drops on the way back in) would have a serious effect, but the below image found in the
TMUX646 S-Parameter Model
suggests there is negligible difference in gain below 1GHz.
I attach an extract from our schematic that hopefully shows our implementation. Please let me know if you have any questions.