I am currently designing an Ethernet RMII circuit and would like to switch the TX+/TX- pair in and out with a RS-485 +/- pair depending on what my customer plugs in. I have the Isolation Transformer for the Ethernet on the TX+/TX- and RX+/RX- pairs, so this switch I would like to happen on the Isolated side near the RJ45 connector. However, the control signals for making the switch would be from our processor on the non-isolated side. My mind says this should be a relay or an optocoupled switch, would this part allow that same functionality?