Is TPS82130 suitable to connect charging capacitors? If there is still voltage in the charging capacitor after a power off, and there is concern that a large inrush current may affect TPS82130 during startup, is this problem present?
Can you recommend an DC-DC covertor (with EN function, 3.3V output, 4A or above output) suitable for connecting charging capacitors.