Tool/software:
Hi All,
Am planning to use TS5A23157DGSR for resistor connect and disconnect resistor,
Below is the example of the circuit
The goal is to connect R498 or R499 to COM2 Pin,
The COM2 pin is connected to another IC(ISET) pin which is an ANALOG INPUT to connector External resistor input to set LED current.
Will this logic work, meaning can TS5A23157DGSR connect and disconnect resistor between NC2 to COM2 or NO2 to COM2