Tool/software: PSPICE for TI
I am trying to simulate this part in PSpice for TI, but receive the following error whenever I try to run a simulation including this part:
I had added the component through the PSpice Part Search, then tried the following alternatives:
These steps did not work for me:
I also tried following the following instructions:
But there are 2 NC pins on the model terminal but under the "symbol pin" dropdown menu it only allows me to select NC for one of the 2, preventing me from continuing
I'm not sure if this is an issue with the model or something else, but support would be appreciated! Thanks