Part Number: CD4066B
Other Parts Discussed in Thread: CD74HC4316, TMUX6211
Tool/software:

Hello, I'm trying to use 2 CD4066BM chips in order to select one of 5 signals (DUT_FILT_CH1, DUT_FILT_CH2, ..., DUT_FILT_CH5) to be connected to "Read_ADC_CH_Filtered" so only 1 ADC Channel is needed.
DUT_FILT_CH1 is a sine wave with an offset near zero volts.
So, problem comes when the signal from (let's say) DUT_FILT_CH1 is connected to Read_ADC_CH_Filtered by putting CONTROL B to HIGH.
The signal at "Read_ADC_CH_Filtered" instantly receives an offset and becomes a sine wave mounted on top of ≈2.2V.
Thought it had something to do with pull-down, so I placed pull-downs on pins 4,8,11,3,9 and 10 but the problem still continued.
Any ideas on what may be causing this ?
Thanks!