This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1308-Q1: TMUX1308QBQBRQ1

Part Number: TMUX1308-Q1

Tool/software:

Hi

I have added a image of the datasheet, which I would like to know when all the pin is on what will be the injection current and also the value of clamping voltage

Thanks

  • Hello Hemalatha,

    The injection current when the switches are on, will be the same values as they are off.  

    The value of the clamping voltage will be a bit above the max recommended voltage level of the device, so around 6V.

    Thanks,

    Nir