This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A3166: Analog switch between RTC CLK and Microcontroller

Part Number: TS5A3166
Other Parts Discussed in Thread: TS5A3167, TMUX1511

Tool/software:

Dear Team,

I am facing an issue and it is described here.

When Microcontroller is off the RTC clock is still on and draining the RTC battery via microcontrollers protection diodes.

I decided to keep an analog switch in between RTC CLK OUT and Microcontroller.

I have two options to power the Switch.

Option 1:

Provide the Microcontroller power rail to switch also.

Once the controller is off Switch also will be off.

My question is will RTC super capacitor discharge via I/O pin of the Switch.

Option 2:

Power switch using RTC super capacitor so that both will be in same power domain.

So that the discharge via i/o protection diodes can be eliminated

Option 3:

May I know you have any better ideas Slight smile

Can I use a signal relay instead of switch.

Regards

HARI