Part Number: TS5A3166
Other Parts Discussed in Thread: TS5A3167, TMUX1511
Tool/software:
Dear Team,
I am facing an issue and it is described here.
When Microcontroller is off the RTC clock is still on and draining the RTC battery via microcontrollers protection diodes.
I decided to keep an analog switch in between RTC CLK OUT and Microcontroller.
I have two options to power the Switch.
Option 1:
Provide the Microcontroller power rail to switch also.
Once the controller is off Switch also will be off.
My question is will RTC super capacitor discharge via I/O pin of the Switch.
Option 2:
Power switch using RTC super capacitor so that both will be in same power domain.
So that the discharge via i/o protection diodes can be eliminated
Option 3:
May I know you have any better ideas
Can I use a signal relay instead of switch.
Regards
HARI