Other Parts Discussed in Thread: TMUX1219, TMUX1119
Tool/software:
Hi Team,
I'm searching a device a drop in replace Diode PI5A4599BCE. We want to drop in replace all the new project and also MPed projects.
I found that our TS5A4624DCKR is P2P with it should be able to replace it.
But customer found the VIH spec in datasheet is different.
In 3.3V supply, our chip request above 2.4V as VIH level, but competitor is about 1.3V.
This will make customer need to check all the MPed project the signal were higher than 2.4V or not.
So my support need is, do we have a P2P part can more close to competitor in spec wise ? The target is drop in replace competitor.
Or do we have TS5A4624 test data can actually meet competitor spec in VIH ?
Thanks!
BR, Kai