Other Parts Discussed in Thread: PCM5102, , CD74HC4052
Tool/software:
I want to use I2S to generate audio through PCM5102 and switch 4 channels using CD4052.
However, malfunction is observed as below.
Problem
1. Audio output is also weak for the rest of the channel that is not selected
2. When testing the channel that is not selected through DMM, the symptoms of weak shorting occur
Inquiry
1. I wonder if there is a problem with the circuit. (I changed the VDD to 3.3V, but the same symptoms occur.)
2. Whether CD4052B is not fit for my purpose