This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Experts, '
Is there any guidelines to follow regarding the input when the TMUX is not powered.
Can i apply input voltage when the supply is not available.
Thank you for the guidance.
Regards,
Sreenivasa
Hi Experts,
Would the below thread referenced answer the query or do you have some additional thoughts?
Regards,
Sreenivasa
Hello Sreenivasa,
The linked thread you provided discusses about the signal on the address pins of the device.
You mentioned applying an input voltage when the supply is not available.
Do you mean a signal going into the address pins or the source pins? If it is the address pins, then there is no issue because of the fail safe logic feature, but if the input is to the source and drain pins (I/O) its a different story. You will need a current limiting resistor on the input for it to work.
Thanks,
Nir
Hello Nir,
Thank you for the inputs.
I realized the links discussed the address pins.
The query was regarding the inputs to S0..S7. I understand the current needs to be limited to 12.5 ma per channel.
Would the input on the S0..S7 cause any back feed on to the supply pins?
Regards,
Sreenivasa
Hello Sreenivasa,
Understood, no the source pins won't cause any back feed on the supply pin due to the injection current control feature the device has.
More information on the injection current control feature can be found in the datasheet
Thanks,
Nir