Tool/software:
I need IEC 60950-1 Certification for SN74CB3Q3257PWR. Please provide the same.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I need IEC 60950-1 Certification for SN74CB3Q3257PWR. Please provide the same.
IEC 60950-1 is a system-level standard, i.e., it applies to the complete device. A chip alone cannot be certified. (And a simple switch like the SN74CB3Q3257 does not provide galvanic isolation and cannot handle high voltages, so it is usually not relevant for such certification.)