This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC4051-Q1: Rthja Conditions considered for the mentioned values

Part Number: CD74HC4051-Q1

Tool/software:

Hi,

I need the conditions that are considered for measuring the Rthja mentioned in the datasheet.

Below are the details I am looking for:

  1. Board type used (is it FR4)
  2. Copper thickness of board in oz
  3. Pad layout: is it minimum recommended pad layout.
  • Hi Harish,

    The datasheet thermal metrics assume the JEDEC standard 2s2p (high-k) PCB, which is an FR4 four layer board.  The thickness of the top and bottom layers is 2 oz Cu and the internal planes are 1 oz Cu.  The trace layout is defined by JESD51-7 and is dependent on the package footprint.

    Regards,

    Kameron