Other Parts Discussed in Thread: SN74LVC1G07
Tool/software:
Hi,
I gave +5V to supply pin.
Input of the channel = 5V.
when the control logic Low = 0V, I got 5V at the output of the channel/switch.
But when I changed the control logic to High = 5V, then also I am getting 5V at the output, i.e the previous output remains at the output even after changing the control logic,
whereas i expect high impedance and hence no voltage there, as the switch is open now for logic 1.
My application requirement is,
for Logic 0 : Input of the channel, i.e 0V or 5V or specifically a short to ground.
for Logic 1: Open or High impedance
Please help me out to solve this. or suggest some other Texas IC to meet my requirement.
Thanks & Regards,
Indira