Tool/software:
Hello, I'm Gunhee. I'm developing an llc resonant converter, and I'm going to use UCC24624 for sr driving. I'm currently using a diode for the secondary side center tap circuit, and I'm trying to use sr for efficiency improvement.
I want to ask you something. I'm trying to use UCC24624ic for sr driving, but I noticed that the sensing range of the VD pin is up to 240V. When I use the diode, it takes about 320V to the voltage across the anode cathode, so can I configure the voltage divider circuit and use UCC24624?
If not, can you recommend a product?