Other Parts Discussed in Thread: TLV741P,
Tool/software:
Hi
As subject, I have measured the NC/NO and COM by multimeter when PCBA is no supply. It is a VF=0.55V between COM and NO/NC.
why?
Is it normal?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Allen,
Can you try either grounding the supplies or tying to VDD and redo the measurements? Your supplies may just be floating and inadvertently turning the FET on and you're actually just reading the threshold of the FET and not the actual diode Vf.
Thanks,
Rami
Hi Rami
I have desoldered this part and re-measured it. It is OK. Attached file is PCB and schematic. Please help to review what happen.

I measure NO/NC and COM because there is cross-talk between NO and NC. Please help review it.
Hi Allen,
Are you asking why you measure a diode when the device was soldered? What was the supply on device when you did this? Is the device functioning properly?
Thanks,
Rami
Hi Rami
I don't know why. I measured it because the oscillator is unnormal. Maybe this IC is brloken when oscillator is turned on.
There are 2 this kind of circiuts on the PCBA, but the other one work normally.



TS5A3160 is supplied by TLV741P.
You can refer to schematic.
VIN=5V, Vout=3.3V @TLV741P
Hi Allen,
I'm sorry, I'm having a hard time following what you're asking here.
Can you please clarify what your issue is?
If you're asking me to look into why there's crosstalk, can you share some scope shots of the crosstalk?
Thanks,
Rami