Tool/software:
Dear supporter,
Would you help check below question , tks!
1. If VCC is 3.3V, B1 and B2 can use below VCC voltage like 1.8V? How about A follows B1 and B2 voltage rail?
2. If VCC is 3.3V, Select pin follows VIN or VIL of VCC, right?
3. If VCC is 3.3V, B1 or B2 could be different single voltage rail (ex: B1: 3.3V ,B2: 1.8V).
4. What relations of voltage domain are along with VCC,B1,B2 and A? And what are the limitations between them?