Tool/software:
Hi team,
Our customer has some questions about injection current control in TMUX1308-Q1. They want to understand this function can work to protect Source pin when it is short to 12V battery.
(Expected use case)

Questions:
1. Please confirm the behavior when an overvoltage is applied to the Sx pin of the device. Our understood that when overvoltage is applied to the Sx pin, the FET in injection current circuitry is turned on. As result, output from D pin will be around 0V. Is the understanding correct?
2. If the understanding of #1 is correct, our understanding is that the voltage of the Sx pin is the voltage divided between the RLIM (external series resistor) and injection current circuitry FET rdson. Please tell us the min and max values of Ron of FET.
3. The output voltage from D pin will be around 0V in the above use case. Is that correct?
4. What are the conditions for the FET to turn on and turn off for overvoltage protection? Could you provide the min/max value and hysteresis voltage for turn on/turn off thershold?
5. For example, considering the case where the S2 pin shorts to battery while S1 pin is selected. Will there be any influence on the D pin? If so, please tell me how to calculate the voltage that affects D pin.
Thank you,
Muwei Zheng