This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6208: TMUX6208 has a bad channel, and the impedance of the channel to the ground is 28Ω. If the Sx port is powered on before a single chip is powered on, will the chip fail?

Part Number: TMUX6208


Tool/software:

TMUX6208 has a bad channel, and the impedance of the channel to the ground is 28Ω. If the Sx port is powered on before a single chip is powered on, will the chip fail?

  • Hello,

    Can you please explain in what do you mean it has a bad channel? Is the device damaged? 

    If the input of the device is powered before the device itself, this might cause damage or failure. 

    If you are looking for a multiplexer that can handle such a case I might be able to recommend one if you can explain a bit more on the application and the requirements. 

    Thanks,

    Nir