This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1104: Can this 1:4 Mux be used for analog signals (ADC signal)?

Part Number: TMUX1104


Tool/software:

Hi Support team 

Can this 1:4 Mux be used for analog signals (ADC signal)?

Red Yen 

  • Hi Red,

    Yes, the mux will act as effectively a resistor with some loading capacitance. So it will work as long as you keep the voltage within the recommended operating range; which is between 0V up to your supply voltage which can be up to 5.5V.

    Thanks,
    Rami