This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX7612: how to create a a low-resistance and repeatable switch

Part Number: TMUX7612


Tool/software:

Dear Team,

I want to create a passive high-precision resistor network for accurate simulation of transducers based on strain gauges with 350 Ohm resistance.

I want to replace the mechanical switches (0%, 10% / 20% ... 100% ) with analog switches. Do you have me some referenc designs?

For calibration, the switch should have a repeatable Ron and Roff at 25°C.

The aim is to reach a accurancy class 0.025 (referencing to https://www.hbm.com/fileadmin/mediapool/hbmdoc/technical/B00333.pdf)

For Data Acquisition Systems TMUX7612 or TS12A4451x or others are better?

Are there better other solutions f.e. with an opamp?

Kind regards

Bernd