This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5177: I need alternative part with functional safety features along with internal MOsfets

Part Number: LM5177
Other Parts Discussed in Thread: LM5157-Q1

Tool/software:

I need an IC that can accept an input range of 6V to 48V and provide a 15V output at 1A. Additionally, the IC should include functional safety features and have an internal MOSFET.