This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4016B: CD40163BE, Counter Single 4-Bit Sync Binary UP 16-Pin PDIP Tube

Part Number: CD4016B
Other Parts Discussed in Thread: TMUX1511

Tool/software:

Hi To Whom May Contact,
I would like to know if this part number CD40163BE,
Counter Single 4-Bit Sync Binary UP 16-Pin PDIP Tube, is still active and procurable?
else, is there a replacement?

Your reply is highly appreciated

Thanks

Brenda Mok

GA EMS Component Engineer

Brenda.Mok@ga.com
  • Hi Brenda,

    This device looks to be active based on ti.com

    However there are many newly developed options that could likely fit your application as well.

    If you would like to explore other options please let me know what supply voltage and more about your use case for this device.

    Other options

    Please let me know 

    Regards,

    Kameron

  • Hi Kameron,

    Thank you for your prompt response.

    Great news. Part number CD40163BE, Counter Single 4-Bit Sync Binary UP 16-Pin PDIP Tube, is still active.

    on the options list you posted, can you please add CD40163BE to the list so that I run the comparison.

    Thanks 

    Brenda

  • Kameron, I am interested parts that are similar to below or better than CD40163BE. I am appreciated if you can recomammad a few parts. Thanks

    Part Number CD40163BE
    Manufacturer Texas Instruments
    Logic Function Counter
    Logic Family CD4000
    Process Technology CMOS
    Number of Count Input Enables  
    Number of Element Inputs  
    Number of Element Outputs  
    Number of Elements per Chip 1
    Number of Selection Inputs per Element  
    Number of Stages 4
    Operation Mode UP Counter
    Output Type  
    Reset Type  
    Direction Type  
    Terminal Count Output  
    Triggering Type  
    Type Binary
    Minimum Operating Supply Voltage (V) 3
    Maximum Operating Supply Voltage (V) 18
    Typical Operating Supply Voltage (V) 3.3|5|9|12|15
    Minimum Operating Temperature (°C) -55
    Maximum Operating Temperature (°C) 125
    Supplier Temperature Grade  
    Maximum Propagation Delay Time @ Maximum CL (ns) 400@5V|160@10V|120@15V
    Absolute Propagation Delay Time (ns) 500
    Propagation Delay Test Condition (pF) 50
    Maximum Quiescent Current (mA) 0.1
    Minimum Storage Temperature (°C)  
    Maximum Storage Temperature (°C)  
    Parallel Enable Input  
    Preset Type Synchronous
    Flammability  
    PDF URL Download PDF
    Flammability Yes
    Flammability Rating UL 94 V-0
    Package  
    Supplier Package PDIP
    Basic Package Type Through Hole
    Pin Count 16
    Lead Shape Through Hole
    PCB 16
    Tab N/R
    Pin Pitch (mm) 2.54
    Package Length (mm) 19.69(Max)
    Package Width (mm) 6.6(Max)
    Package Height (mm) 5.08(Max) - 0.51(Min)
    Package Diameter (mm) N/R
    Package Overall Length (mm) 19.69(Max)
    Package Overall Width (mm) 10.92(Max)
    Package Overall Height (mm) 5.08(Max)
    Seated Plane Height (mm) 5.08(Max)
    Mounting Through Hole
    Package Weight (g)  
    Package Material Plastic
    Package Description Plastic Dual In Line Package
    Package Family Name DIP
    Jedec MS-001BB
    Package Outline Download PDF
    Manufacturing  
    MSL N/R
    Maximum Reflow Temperature (°C) N/R
    Reflow Solder Time (Sec) N/R
    Number of Reflow Cycle  
    Standard  
    Reflow Temp. Source  
    Maximum Wave Temperature (°C) N/A
    Wave Solder Time (Sec) N/A
    Wave Temp. Source  
    Lead Finish(Plating) SnPb
    Under Plating Material N/A
    Terminal Base Material N/A
    Number of Wave Cycles  
  • Hi Brenda

    I think this list of parts is particular a good group to evaluate if you want to replace the Cd4016B in the future and the main selection points between these different devices is supply voltage and the package size that you want to use in your application.

    Our teams newest device called the TMUX1511 is used in systems that have a 1.5V to 5.5V supply and need small package options.

    Please let me know if you need any help and the list above has the cd4016B in it

    Regards,

    Kameron

  •  TMUX1511 is for SMT.

    CD40163BE has 16 pins, for Through Holes. i am looking for a replacement of CD40163BE.

    CD4016BE has only 14 pins.

    does CD40163BE very active?

  • Ok understood,

    Yes the CD4016Be  is active and a p2p replacement would be the CD4066BE

    Both of these devices have 14 pins

    Please let me know if any other assistance is needed

    Regards,

    Kameron

  • I do not need the CD4016BE but CD40163BE.

    Is CD40163BE active and procurable? else is there a replacement?

    CD40163BE, Counter Single 4-Bit Sync Binary UP 16-Pin PDIP Tube

  • Ok after looking i found that device is actually discontinued and I couldn't find that particular device on ti.com

    However the CD4016BE is the best replacement for that device and has the same package size and functionality.

    Is that acceptable?