This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1511: What is the power off isolation over frequency?

Part Number: TMUX1511


Tool/software:

In the data sheet, Figure 21 shows the "Off Isolation vs. Frequency".  I need to know the "Powered Off Isolation vs. Frequency".   Can you provide this?  In my application, I need an analog switch that disconnects a 50 ohm receiver from a transmission line when the board is unpowered.  The bit rate of the signal is around 100Mbps.  I'm hoping for significant isolation up to 1Ghz. I specifically care about unpowered isolation.

BTW, I'm surprised how bad the powered off isolation is above 200Mhz for a part that is advertising 3Ghz bandwidth.  This seems like false advertising.  Am I missing something?  

Thank you.