This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS12A4515: TS12A4515

Part Number: TS12A4515

Tool/software:

Dear TI technical support, 

 

I used TS12A4545 analog switch for my current design. I am using four of these switchesTS12A4514 and TS12A4515 to switch from one sensor to another. I am using one pair of these switches at one side and an another pair at other side. The control signal is distributed then to these four switches by just pulling the same CTRL traces to individual switches. Is there any suggestion about driving such multiple loads? I am plannig to use this switch in a environment where there is a quite high temperature easily around 100°C all the time. It is a production site. The switching should happen reliably back and forth and there should be no turning on or off at the same time. It would be great if you comment on that and do some suggestions. 

I appreciate you very much for your great cooperation. 

 With the best 

Sonom Olonbayar