Tool/software:
Hello,
I have a few questions regarding the use of the TMUX in my application:
-
The datasheet mentions 1.8V logic compatibility. Will it also support 5V logic levels without issues?
-
For unused input channels and the VSS pin, is it advisable to tie them to GND?
-
When the power supply is not connected, I notice the output pin shows some floating/garbage voltage (around 0.1–0.3V). What could be causing this, and would using a pull-down resistor help? Do you have any suggestions to resolve this behavior?
-
My setup involves three types of command inputs: 0–5V, 0–10V, and 0–20mA. I convert the 0–20 mA signal to voltage and feed all three signals to the MUX inputs. However, when I try to replicate the setup, I observe voltage drops across the other inputs (0-5 and 0-10 V). What could be causing this interference or drop, and how can it be resolved?
-
Since I only have three input channels to choose from, I don't require all three select lines. Can I safely tie the A2 (select input) to GND and use only A0 and A1?
Thank you,
Showrya