This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1204: Gain Settings for OPA

Part Number: TMUX1204
Other Parts Discussed in Thread: OPA2990, , TMUX1208

Tool/software:

Hello 

Customer plans to use TMUX1204 (x 2pcs) to do the Gain setting of the OPA2990 in Resolver application as below circuitry. Is there any side effect or any need to pay attention? Please help to check on this circuitry!

Application: Resolver for AC inverter

Resolver IC: AS12S1210

R2 Value is 8.5K to 31K Ohm. TMUX1204's Rds,on is about 4.9Ohm. there should have no impact on Gain value settings. 

Regards

Brian