Tool/software:
We are using SN74CBTLV16292 for muxing application and in case the output pin is not used then there is an internal pull down which gets activated which is leading to Bus contention as the same pin is connected to an external working device and leading to a failure. Is there a way that this internal pull down can be eliminated which when I looked at doesn't feel is possible. If internal pulldown cannot be eliminated then can you suggest an alternative IC which is exactly pin compatible but without internal pulldown so that the IC is easily replaceable. This is holding up a major release and a prompt reply is appreciable.