This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
One of my customers is looking at the following characteristics for TS5A22364DGSR:
1. Signal to Noise Ratio with reference to 0 dBm level measured at 1 kHz
2. % of Harmonic distortion of the line level audio output across the audio bandwidth 20H-20kHz
3. Line level audio output dynamic range in reference to 0 dBm level measured at 1 kHz
4. Stereo pairs cross-talk at maximum output across the frequency bandwidth
and the following characteristics for TPA4411:
TPA4411:
Dynamic range of the Amplifier - in reference to 0 dBm level measured at 1 kHz.
Can you please help me get the following data for the two devices?
Kind Regards,
Vaibhav Shinde
Hi, Vaibhav,
the DNR of the TPA4411 is about 98 dB. I am not sure about the TS part, let me see if I can find the proper forum for that. BTW, that part is pretty old, we have much newer, cheaper, better DirectPath HP amplifiers now...
-d2
Hello Don,
Thanks a lot for the information and also for directing my query to the appropriate place.
I will look into the newer DirectPath HP amplifiers on ESP and try to promote them with our customers.
Kind Regards,
Vaibhav
Hi, Vaibhav,
1. The THD (Total Harmonic Distortion) spec is listed in the datasheet. The TS5A22364 has better than 0.01% performance under different supply rangees.
2. X-Talk spec is also listed in the spec. The performance is better than -75dB.
We don't ahve characterization data for SNR and Dynamic Range unfortunately.
Thanks,
David