Tool/software:
Hello, I have an application where a pair of analog switches (TS3A24159) are used as a multiplexer to connect two individual 3-Wire PT100 RTD probes to a single RTD-to-Digital Converter. These RTDs are standard class A units. I'm switching between the two RTDs once every 500ms and I'm reading a difference of ~1.5-2 °C between the two probes. The difference gets worse when the PCB is heating up.
What could be the cause here? Is it the Ron variation on the switch channels causing the issue?