This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX121: 2:1 MUX IC technical details

Part Number: TMUX121
Other Parts Discussed in Thread: TS3DV642

Tool/software:

Dear Team,

Can you please suggest a 1 channel 2:1 MUX IC which supports HDMI 2.0 signals

I have 2 differential pair HDMI inputs signals to the MUX IC and choose between those two signals as output.

Kindly suggest a part for my requirement at the earliest.

Regards,

Abhishek

  • Hi Abhishek,

    TMUX121 may work, depending on your voltage. My understanding was that HDMI 2.0 was 5V. If so, then TMUX121 won't work here since it only supports up to 3.6V on the I/O's.


    TS3DV642 will work for up to 5.5V on the I/O's. 

    Thanks,
    Rami