This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX136: TMUX136

Part Number: TMUX136
Other Parts Discussed in Thread: TMUX1574

Tool/software:

is it support the sd 3.0 signal speed?

can i use this for sd express application?

  • Hi,

    Yes the TMUX136 should be fine for this application as the 3.3V or 1.8V io signals are are ok for this device.( This device can handle 3.3V or 1.8V on its io pins)

    In addition this device bandwidth is 6GHz which is more than enough for the max frequency of 208MHz which is for  SD3.0

    Another device that will be good for this application is the TMUX1574 which also has the io voltage range and bandwidth to support this application.

    Please let  me know if you have any other questions.

    Regards,

    Kameron