This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1208: TMUX1208 with 4-20mA loop signals

Part Number: TMUX1208
Other Parts Discussed in Thread: RCV420, TMUX7208, INA180, TLV9001

Tool/software:

Dear TI Support,

I need to interface Sensors in an industrial gloove box, O2 Sensor with passive with 2 wires 4-20mA output and H2O Sensor active with 3 wires 4-20mA.

These sensors are supplied with external +24V.

I would like to know if i could use your TMUX1208 for multiplexing 4-20mA input signals to send to a RCV420 4-20mA loop receiver?

The RCV420 is supplied with +/-15V .

Thanks for your help,

Best Regards,

Marc MORAND