TMUX1575: I2C signal mux

Part Number: TMUX1575

Tool/software:

Hi team,

Does is OK for TMUX1575 use as I2C mux signal switch?

Customer get a pair of I2C, and another 2 signals, need to switch between 2 devices, does it OK for TMUX1575 as this function?

Regards,

Will

  • Hi Will,

    The TMUX1575 has a high enough bandwidth to support what you need. The only concern is the voltage, as long as you are within the specifications from the datasheet (1.08V to 3.6V), then there are no concerns on my end.

    Thank you,

    Arya