Tool/software:
In section 8.3.6.2 of the datasheet, it outlines the conditions and reaction of the part when a channel is selected, and an overvoltage event occurs. When this happens, the datasheet says that the protection circuitry is partially active. Does this mean that it is active only enough to act as a current sink in order to pull down the output to Vdd? Other than the current limiting resistor on the input, will I need further downstream protection, or is the ground shunt enough? Thank you.