TS3DS10224: Can I use TS3DS10224 part for RS-422 application ?

Part Number: TS3DS10224


Can i use this part for RS-422 loop back application

  • Hello Suryaseshu,

    The TS3DS10224 can pass signals up to its supply, which is 3.6V max.

    What voltage levels are the RS-422 signals you want to pass through it? Also what is the frequency? 

    TS3DS10224 has a rated bandwidth of 1.2GHz, which should be enough but I want to confirm.

    Thanks,

    Nir