This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need a recommendation for a low-cost, low-power, low-speed N.C. SPST switch.
I have a circuit that I want to switch off the battery power to when an external 5.0V is applied from a USB cable:
The switch (shown in the red box) needs to connect the Li-Ion battery (3.2-4.1V) to power the small circuit (with only 2 active components a schottky diode and a low-power D latch SN74AUP1G80. The switch would be SPST normally closed and would open when the USB power is supplied (~5.0V but could be 4.5-5.5 per USB spec).
Thanks in advance!
Kind regards,
Kevin Kreger
Hello Kevin,
I would recommend the TS12A4515 for your application as long as the current through the switch does not reach the 20 mA maximum current through any port as specified by the datasheet.
Regards,
Andrew
Hi Andrew
The LVC1G80 has the Ioff feature that sets the I/O's to high impedance when VCC is 0V. It would not work if it is floated. I would suggest a SPDT instead and switch Vcc to 0V. This would help keep you current low. http://www.ti.com/product/sn74lvc1g3157 should work
Hello all,
Thank you Chris that was a good catch!
Kevin in light of Chris' insight I would recommend you look into the TS5A2053 as a SPDT solution instead of a SPST, with battery tied to NC and 0V tied to NO.
Regards,
Andrew
Hi Chris,
Thanks so much for your design advice! I have incorporated the switch and just have a few questions and comments:
Here is how I believe the circuit should be implemented based upon your advice:
Chris, I'm not sure I understand all of your comment to Andrew. However, based on the reasoning above I do not have to worry about the case of Vcc = 0.
Thanks again to both of you for helping out with this design!!!!
Kind regards,
Kevin Kreger
PS: Which forum is appropriate to get a recommendation for ~0.7V surface mount diode (D2)
Hi Guys,
I guess I totally f*d that up! because Andrew advised that I tie 0V to NO and battery to NC. Here is something closer to your advice:
In addition, here are my newly configured questions
THANKS!
Kind regards,
Kevin
THANKS!
Hi Chris,
First of all many thanks for your careful analysis! I want to go over your points and respond to each, thank you in advance for your kind patience: