Hello. I currently use the 74AUC2G66 for switching 1.8V signals. For BOM part variant reduction, I would like to continue using this part for some 3.3V signal switching I need to do. I see that the part has an absolute voltage range up to 3.6V. Is there any reason I should be concerned with running this part at an operational 3.3V instead of the "recommended" 2.7V?